earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: Basic Functionality
12/2/2024

Styling a Certain Event in the Events Pane or Event View

You style the appearance of an event in the Events pane or Event View to easily detect the event when it occurs.

Show More
action_close

You can style certain events to bring out those that are of more interest than other events listed in the Events pane and Event Views. To style a specific event, you first have to create a condition that is associated with the events you want to style. An event can be styled with a unique background color, font, and font color.

For example, you can style all events where an alarm is acknowledged. To separate this event from others you configure, change the background color to dark green and the font color to white. All other events have the default style which is a white background and black font color.

If an event fulfills the condition criteria in more than one of the configured event criteria, it is the event style with highest priority in the Events View Style dialog box that is applied to the event.

Events styling does not apply to WebStation and does not affect the events in WebStation.

Event View standard filter and layout

A standard layout defines the columns that are included in the Alarms pane, Events pane, Alarm View, or Event View, the order in which they are displayed, whether or not the alarms or events are grouped in any way and whether they are displayed in an ascending or descending order. A standard filter defines the conditions that have to be met before the alarms or events are displayed in the pane or a View. The standard layout and filter is saved for the pane or View to which you made the changes. The standard layout and filter is displayed for all users of the the EcoStruxure BMS.

For more information, see Alarm View and Event View Standard Filter and Layout .

Events styling does not apply to WebStation and does not affect the events in WebStation.

To style a certain event in the Events pane or Event View
  1. Click somewhere in the Events pane or Event View to make sure the pane or dialog box is in focus.

  2. On the Actions menu, click Edit the style of associated events .

  3. In the Event Styles dialog box, click the Add style

     
    action_zoom_plus_stroke
    button.

  4. In the Condition box, click the Browse button.

  5. In the Select Conditions dialog box, click the Add condition button

     
    action_zoom_plus_stroke
    and select an event category.

  6. Enter the settings of the event category associated with the event you want to style.

    Note:
    • You can add several event categories to specify the event in detail.

  7. Click the Add row button

     
    action_zoom_plus_stroke
    to add another condition of the same type.

  8. Click OK .

  9. In the Event Styles dialog box, in the Background color box, click the Browse button.

  10. In the Color dialog box, select the color for the background of the event row in the Events pane or Event View.

  11. Click OK .

  12. In the Font color box, click the Browse button.

  13. Select the color for the font of the event in the Events pane or Event View.

  14. Click OK .

  15. In the Font box, click the Browse button.

  16. In the Font dialog box, select the font, font style and size that you want to display the certain event text in.

  17. Click OK .

  18. In the Event Styles dialog box, click OK .

You can add several event styles to different associated events.

  • Events Pane and Event View Customization
  • Creating a Filtered Event View
  • Event Styles Dialog Box
  • Event Filter Conditions