earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WorkStation
Functionalities: Graphics
12/19/2024

Zooming In an Area of a Graphic

You zoom in a graphic to view a part of the graphic in more detail.

Show More
action_close

You use graphics to display building overviews, display the status of detectors and alarms, display the value of sensors, or change setpoints. A graphic can also contain links to trend charts, trend log lists, Internet sites, or views in WorkStation and WebStation.

A graphic that contain links to documents, such as Microsoft Word or Adobe PDF, can be opened in WorkStation and WebStation. The associated programs, in this case Microsoft Word or Adobe Reader, has to be installed on the computer running WorkStation or WebStation.

 
action_zoom_plus_stroke A Graphic with links and interactive components like gauges in WorkStation
Figure: A Graphic with links and interactive components like gauges in WorkStation

Fire Graphic Headers

If a default graphic is defined in the fire detection system configuration, the Home button

 
action_zoom_plus_stroke
in the fire graphic header displays the default graphic.

If a navigation menu is created in the fire detection system configuration, the Navigation button

 
action_zoom_plus_stroke
in the fire graphic header displays the navigation menu.

Fire Graphic Menus

The graphic menus in EcoStruxure Fire Operation are used to display alarms and alerts in a graphic. The menus are also used to apply commands on either loop devices and zones in a graphic or on the fire detection system.

For more information, see Fire Graphic Menus .

Sets of Icons in Fire Graphics

There are two sets of icons in fire graphics, default icons and Swedish icons.

For more information, see Sets of Icons in Fire Graphics .

To zoom in an area of a graphic
  1. Click the Zoom In button

     
    action_zoom_plus_stroke
    .

  2. Drag the magnifier over the area in the graphic you want to increase in size.

  • How Graphics Work in Fire Operation
  • Graphics Toolbar
  • Resetting Zoom in a Graphic
  • Zooming Out from a Graphic