earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WorkStation
Functionalities: Basic Functionality
12/2/2024

Resetting the Workspace Layout

You reset the workspace layout to return to the default workspace layout for your user account.

Show More
action_close

In WorkStation you can customize your workspace to some extent. You can, for example, decide where workspace components, such as, Alarms are displayed.

You can configure the workspace layout, for example, to display different workspace items on different monitors or to change the size of a pane to improve readability. When you save the modified workspace layout, it is saved on the local computer. If you log on to WorkStation on another computer you cannot access the customized layout. The modified workspace layout is displayed the next time you log on to WorkStation.

You can switch the following bars on or off:

  • Address bar

  • Menu bar

  • Toolbar

  • Status bar

  • Search bar

  • History bar

For each window, pane, or work area in the workspace the user can modify the following:

  • Auto hide on/off

  • Closed on/off

  • Floating on/off

  • Position

You can reset a modified workspace layout on the local computer. In this case, you return to the default workspace layout that applies for your user account.

To reset the workspace layout
  • In WorkStation, on the View menu, click Reset workspace layout .

The workspace layout is reset to the default workspace for your user account.

  • Customization
  • View Menu