You change the PIN of the SpaceLogic Bluetooth Adapter for best security practices. The Bluetooth Adapter PIN is engineered to a default code of 333666 and should be changed to a secure code before you perform device commissioning. You configure the password for Bluetooth access in the RP controller.
Connect to the Adapter. For more information, see Connecting to a Controller through Bluetooth .
In the Bluetooth Device Management page, in the PIN field, type the new PIN and click Update .
The Commission mobile application returns to the Bluetooth Devices page. On the Adapter, push the LED button to initiate pairing.
In the Commission mobile application, select the Adapter and click Connect .
In the Bluetooth Device Management page, click Connect .
Your mobile device or Window laptop prompts you for the Adapter PIN. Enter the new PIN and click Pair .
Be sure to enable the Sensor bus property on the RP controller Settings object. Otherwise, the Bluetooth adapter will not operate. For more information, see BACnet/IP Controller Settings Properties – Basic Tab .
When you see the Configure page, you have successfully connected to the controller.