earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-C, AS-B, AS-P, WorkStation, Project Configuration Tool
功能: 基本功能
产品版本: 1.8, 1.9
2024/10/2

Duplicating a SmartStruxure Server Device Using Restore 

You duplicate a SmartStruxure server from a backup set using Restore when you want to reuse configuration data from a backup set in a standalone SmartStruxure server device.

重要:

The locally stored backup set and the SmartStruxure server device need to have the same password.

Restoring with new ID does not work if the database contains a BACnet interface.

显示更多
action_close

You can use the Restore function to re-use the configuration data from a backup set in a new standalone SmartStruxure server device. Rather than manually configuring your preferred SmartStruxure server device configuration, you can save time and configure the standalone SmartStruxure server device from a backup set.

The backup set used can originate from a SmartStruxure server device that is or has been part of a multi-server configuration.

To store a backup set in another location, you save a selected backup set to a folder on your WorkStation PC or network drive.

有关更多信息,请参阅 Backup Sets .

Protocol Compatibility

The restore function to re-use configuration data from a backup set is supported for all Building Operation supported protocols, except for BACnet and b3 BACnet.

LonWorks Devices Neuron IDs deleted on duplicated SmartStruxure server device

The LonWorks devices connected to the SmartStruxure server device are not the same as the LonWorks devices that are to be connected to the duplicate. When you create a duplicate from a SmartStruxure server device, all Neuron IDs in the duplicate are deleted. This is also a way to avoid network conflicts.

After you created the duplicate, you add new Neuron IDs to the duplicate. You then commission all LonWorks devices on the new SmartStruxure server device.

有关更多信息,请参阅 LonWorks Device Workflows .

Password deleted on duplicated SmartStruxure device

When you duplicate a SmartStruxure device from a backup set all passwords are deleted on the duplicate for security reasons. The only exception is the default admin password. The administrator is forced to change the password at the first logon at the duplicate. All users must be given new passwords by the administrator.

Multi-server Site

To create a new SmartStruxure server device in a multi-server configuration, using a locally stored backup set, you need to make the backup set available for restore on the multi-server system. You add a new SmartStruxure server device to the Enterprise Server and select the backup set in the Create Object Wizard.

有关更多信息,请参阅 Creating a SmartStruxure server device from a Backup Set .

Standalone SmartStruxure Server Device Site

You use a locally stored backup set to duplicate another SmartStruxure server device configuration in a standalone SmartStruxure server device. You then import the backup set to a client and restore to the new standalone SmartStruxure server device.

有关更多信息,请参阅 Duplicating a SmartStruxure Server Device Using Restore  .

Duplicate SmartStruxure Server Device from a Backup Set Workflow

Use the following workflow to duplicate a SmartStruxure server device from a backup set.

 
action_zoom_plus_stroke Duplicate SmartStruxure server device using restore flowchart
图: Duplicate SmartStruxure server device using restore flowchart
Backup a SmartStruxure server device

Backup a SmartStruxure server device that has the configuration you want to use in the new standalone SmartStruxure server device.

有关更多信息,请参阅 Backing Up SmartStruxure Servers Manually .

Copy backup set to local directory

Copy the backup set to a local directory.

有关更多信息,请参阅 Saving a SmartStruxure Server Device Backup Set to Another Location .

Log on to standalone SmartStruxure server device

Log on to a new standalone SmartStruxure server device.

有关更多信息,请参阅 以楼宇管理系统用户身份登录工作站 .

Import backup set

Import the backup set.

有关更多信息,请参阅 Importing a Backup Set to SmartStruxure Server Device .

Restore SmartStruxure server device using Restore configuration with new IDs

Use the Restore configuration with new IDs function to duplicate the configuration data from the imported backup set in the new standalone SmartStruxure server device. The communication settings from the backup set are not duplicated.

有关更多信息,请参阅 Duplicating a SmartStruxure Server Device Using Restore  .

重要:

When you restore a standalone SmartStruxure server device, you are logged off and need to log on manually after the restore is complete.

To duplicate a SmartStruxure Server Device using restore
  1. In WorkStation, in the System Tree pane, select the server where you want to duplicate configuration data from a backup set.

  2. On the Actions menu, click Restore .

  3. In the Available restore points list, select the backup set.

     
    action_zoom_plus_stroke
  4. Select Restore configuration with new IDs checkbox to re-use the configuration data from the backup set in a new standalone SmartStruxure server device.

  5. Click Restore .

  6. Click Yes .

  7. Click Close .

  • Duplicate SmartStruxure Server Device from a Backup Set
  • Restore
  • Restore Options Dialog Box
  • Importing a Backup Set to SmartStruxure Server Device
  • Backup Set Text is Red