earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: WorkStation, WebStation
Functionalities: Basic Functionality
Product version: 2024, 7.0, 7.1
10/30/2025

Modify Values

arrow1_rotationForced Values arrow1_rotationAdd and Change Units and Prefix

You can change and force values using a graphic or the Properties pane. Using the Watch pane, you can dynamically monitor a value.

Forced Values

When you force a value, you override all input from the system. For example, if a schedule is set to enable a device at 09:00, but you want to enable it at 08:00, you can force the enablement at 08:00.

For more information, see Forced Values .

Add and Change Units and Prefix

You can add or change units and prefixes on values using WebStation.

For more information, see Adding or Changing a Unit and Prefix for a Value in WebStation .

  • WorkStation Overview
  • Building Operation WebStation Overview
  • Fire Operation WebStation Overview
  • Value Presentation
  • Forced Values
  • Watch Pane and Watch View
  • Watch Pane and Watch View Toolbar
  • Graphics Toolbar
  • Adding an Object to the Watch Pane or a Watch View
  • Removing an Object from the Watch Pane or a Watch View
  • Changing a Value in a Graphic