earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: WorkStation
Functionalities: Basic Functionality
Product version: 2024, 7.0
10/30/2025

WorkStation Overview

arrow1_rotationLog on to WorkStation arrow1_rotationSystem Registration arrow1_rotationUser Experience arrow1_rotationCustomization arrow1_rotationBasic Functions arrow1_rotationHandle Values arrow1_rotationHow Alarms Work arrow1_rotationHow Events Work arrow1_rotationHow Schedules Work arrow1_rotationHow Trend Logs Work arrow1_rotationHow Graphics Work arrow1_rotationHow Documents Work arrow1_rotationWorkStation Help

WorkStation is your main interface to your EcoStruxure BMS. You use WorkStation to perform all work on a daily basis in the EcoStruxure BMS.

Log on to WorkStation

You log on to WorkStation to securely access the functions in WorkStation. You log on to WorkStation as a Windows user or an EcoStruxure Building Operation user. Your system administrator decides which type of user you log on as.

For more information, see Log on to WorkStation or WebStation .

System Registration

As the owner, you register your EcoStruxure BMS to ensure that you are informed in the unlikely event of any critical cybersecurity vulnerabilities that have been discovered in the version you are running, and your system integrator for some reason is unavailable. The information we collect makes potential onboarding to other digital services from Schneider Electric quicker and easier. The information will also help Schneider Electric make more informed decisions in future product development.

For more information, see System Registration .

User Experience

The Work area in the EcoStruxure Building Operation user interfaces may vary depending on how it is set up. A typical EcoStruxure Building Operation workspace contains panes and views.

For more information, see User Experience .

Customization

In WorkStation you can customize your workspace to some extent. You can, for example, decide where workspace components, such as Alarms, are displayed.

For more information, see Customization .

Basic Functions

To get a better view of the objects in views and lists, you can use a number of functions like filtering, grouping, and sorting.

For more information, see Basic Functions .

Handle Values

You can change and force values using a graphic or the Properties pane. Using the Watch pane in WorkStation, you can dynamically monitor a value.

For more information, see Modify Values .

How Alarms Work

You are notified by alarms when some important event occurs. For example, if the temperature is too low or too high in a building, if a window is open, or if a fire device is out of order. The system administrator sets up the alarms and decides to whom the alarm is sent.

For more information, see How Alarms Work .

How Events Work

All system events, as well as information and circumstances, are recorded in the Event log. These event records can be viewed in the Events pane or in an Event View.

For more information, see How Events Work .

How Schedules Work

Schedules are used to schedule the operation of parts of the BMS, such as a device or a setpoint. For example, a you can set up a schedule to make a device to operate between 08:00 and 17:00 every workday.

For more information, see How Schedules Work in Building Operation .

How Trend Logs Work

You use trend logs to record values from devices, such as sensors. A trend log can also log consumptions, such as energy consumption or water consumption.

For more information, see How Trend Logs Work .

How Graphics Work

You use graphics to display building overviews, display the status of detectors and alarms, display the value of sensors, or change setpoints. A graphic can also contain links to trend charts, trend log lists, Internet sites, or views in WorkStation and WebStation.

For more information, see How Graphics Work in Building Operation .

How Documents Work

You can open documents stored on an EcoStruxure BMS server using the default program associated with the file type. For example, a txt-file opens Notepad and a ppt-file opens PowerPoint.

For more information, see How Documents Work .

WorkStation Help

WorkStation Help provides you with information on how to handle and understand the EcoStruxure BMS.

For more information, see WorkStation Help .

  • Work Interface Overview
  • Log on to WorkStation or WebStation
  • User Experience
  • Customization
  • Basic Functions
  • Modify Values
  • How Alarms Work
  • How Events Work
  • How Schedules Work in Building Operation
  • How Schedules Work in Fire Operation
  • How Trend Logs Work
  • How Graphics Work in Building Operation
  • How Graphics Work in Fire Operation
  • How Documents Work
  • WorkStation Help
  • Utilities
  • Starting WorkStation
  • Exiting WorkStation