Prior to using the eCommission SmartX Controllers mobile application at a job site, there are certain preparations that must be made. Complete the following tasks, as well as any additional tasks that may be necessary.
|
Task at Job Site |
Preparation |
|
To use the eCommission application at the job site |
Download the eCommission application to the mobile device and then activate the application (requires Internet access). For more information, see Downloading and Starting the eCommission SmartX Controllers Mobile Application . For more information, see Launching and Activating the eCommission SmartX Controllers Mobile Application . |
|
To connect the eCommission application to the SmartX IP controllers |
Consider the connectivity requirements needed for the job site, for either option: connect by wire or connect wirelessly. For more information, see Connection and Architecture Options . |
|
Download application images to SmartX IP controllers at the job site |
Copy the application images onto the eCommission application mobile device. For more information, see Transferring an Application Image File to a Mobile Device . |