Start the eCommission SmartX Controllers mobile application to perform commissioning, flow balance, and checkout operations on SmartX IP controllers.
Download and then install the eCommission SmartX Controllers application to the mobile device from Google Play, the Apple App Store, or the Microsoft Store.
eCommission SmartX Controllers is the name of the application used in the download sources.
On the mobile device, start the eCommission application.
In the Login view, in the Username box, type your username.
In the Password box, type your password.
Tap or click Login .
In the Select Connection view, tap or click the WiFi button
In the UDP Port dialog box, accept the UDP port number of the BACnet internetwork as given or type a different UDP port number. If you are uncertain, accept 47808 and then tap or click OK .
If you are unable to connect, the UDP port number may be different from the default value. Consult with the EcoStruxure system administrator and then type the correct port number in the UDP Port box.
In the Select BACnet Network dialog box, select one or more networks.
Tap or click DISCOVER DEVICES .
Now you are ready to use the eCommission application to interact with the SmartX IP controllers.