earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Commission, IP-IO , MP-C, MP-V, RP-C
Functionalities: Engineering, BACnet/IP devices
Product version: 2022, 2023, 2024, 7.0
9/12/2024

Connecting to Network of BACnet/IP Controllers by Wire

Running the Commission mobile application on a Windows laptop computer, you can connect directly to an Ethernet port on a networked BACnet/IP controller, or use an Ethernet switch to connect to a group of controllers.

Show More
action_close

Use this workflow to connect the Commission mobile application to BACnet/IP controllers.

Related information can be found in the sections that follow the flowchart.

 
action_zoom_plus_stroke Commission mobile application connection workflow
Figure: Commission mobile application connection workflow
Download, install, and log on to the Commission mobile application

Download, install, and log on to the Commission mobile application, and then accept the Terms of use agreement.

For more information, see Logging on to the Commission Mobile Application .

Power up the controllers

Power up the BACnet/IP controllers.

For more information, see Powering Up MP-C .

For more information, see Powering Up MP-V .

For more information, see Powering Up an RP-V Controller .

Prepare a wired or wireless connection for Commission mobile application

Prepare a wired or wireless connection for use with the Commission mobile application mobile device.

Connection Type

More Information

Wired connection to a single controller

For more information, see Connecting to Single BACnet/IP Controller by Wire .

Wired connection to a network of controllers

For more information, see Connecting to Network of BACnet/IP Controllers by Wire .

Wireless connection to a network of controllers via a WiFi router

For more information, see Connecting to Network of BACnet/IP Controllers through WiFi Router .

Wireless connection to a network of controllers via a wireless access point

For more information, see Connecting to Network of BACnet/IP Controllers through a Wireless Access Point .

Start the Commission mobile application and discover controllers

Start the Commission mobile application and then discover the BACnet/IP controllers on the network.

For more information, see Logging on to the Commission Mobile Application .

To connect to a network of BACnet/IP controllers by wire
  1. Configure the network connections on the Commission mobile application computer and the BACnet/IP controllers:

    For more information, see Configuring BACnet/IP Controller Settings .

    • If the network contains a DHCP server, configure these network connections for DHCP addressing.

    • If the network does not contain a DHCP server, configure these network connections for static IP addressing.

  2. Connect an Ethernet cable between the Commission mobile application computer and Port 1 of an BACnet/IP controller on the network. If you are using an Ethernet switch, connect the computer and the controllers to the switch, using Ethernet cables.

  3. In the Commission mobile application, on the Home page, click IP Network , select a network adapter, and discover devices.

  4. In the Device List view, select the BACnet/IP controllers to make the connections.

Using the Commission mobile application, you can now perform tasks on the connected BACnet/IP controllers as needed.

  • Connection Workflow for the Commission Mobile Application
  • Configuring BACnet/IP Controller Settings