earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: RP-C, RP-C-EXT-0-10V-4, RP-C-EXT-0-10V-4-PD, RP-C-EXT-BL-2-LV-PD, RP-C-EXT-BL-4-HV-PD, RP-C-EXT-BL-SMI-2-LV-PD, RP-C-EXT-BL-SMI-4-HV-PD, RP-C-EXT-DALI, RP-C-EXT-DALI-M-PD, RP-C-EXT-REL-4, RP-V
Functionalities: Hardware
Product version: 2023, 2024, 7.0, 7.1
10/20/2025

Removing an External Connector from an RP Controller Expansion Module or RP-C-16C-F-230V Controller

You remove an external connector from an RP controller expansion module to disconnect lights, blinds, dry contact digital inputs, or AC power from the module. You remove an external connector from an RP-C-16C-F-230V controller to disconnect 230 VAC power from the controller, to disconnect an external 24 VAC/VDC power supply, or to disconnect equipment controlled via the SSR outputs and/or universal inputs/outputs.

Show More
action_close

The RP controller expansion modules have PCB mounted connectors for the power input, outputs, and digital inputs. The PCB mounted connectors mate with pluggable connectors:

  • The light modules, blind modules, and the RP-C-EXT-REL-4 relay module have mechanically keyed and color-coded connectors, which allows the matching external connectors to be plugged in on site quickly and easily.

  • The CRS-HH-REL-10 relay module has PCB header connectors for pluggable screw terminal blocks, which are easy to install and remove from the device.

Light Modules, Blind Modules, and RP-C-EXT-REL-4 Relay Module

The pluggable connectors mean time savings and cost reductions for the installation, compared to wiring terminal blocks on site. The connectors can quickly and easily be plugged together on site.

The RP controller expansion modules use 2, 3, 4 or 5 pole connectors for the different inputs and outputs. The 4-pole connector has a 5-pole frame.

The connectors are mechanically keyed, which means the following connections cannot be made:

  • A connector for AC mains and high-voltage applications cannot be plugged into a connector for low-voltage applications.

  • A connector for low-voltage applications cannot be plugged into a connector for AC mains and high-voltage applications.

The matching connectors are locked together.

The connectors are also color-coded to help the installers and electricians to choose the correct, matching external connector. The connectors are color-coded:

  • Black: For AC mains power applications such as power supply input, blind high-voltage outputs, SMI (HV) blind outputs, and relay outputs.

  • Pastel blue: For dimming applications such as DALI inputs/outputs and 0-10V light outputs with power distribution.

  • Light blue: For low-voltage applications such as blind low-voltage outputs (24 VDC), 0-10V light outputs without power distribution, SMI LoVo (LV) blind outputs, and digital inputs (5 VDC).

 
action_zoom_plus_stroke Color-coded connectors (example)
Figure: Color-coded connectors (example)

The matching external connectors are not provided but need to be ordered separately from Schneider Electric. For more information, see Required External Connectors for the RP Controller Expansion Modules .

CRS-HH-REL-10 Relay Module

The CRS-HH-REL-10 relay module uses pluggable screw terminal blocks, which are easy to install and remove from the device.

The terminal blocks are delivered in a plastic bag with the device.

The terminal blocks are used as follows:

  • 2-pole terminal blocks (x10) for the relay outputs

  • 9-pole terminal blocks (x2) for the digital inputs

Table: Recommended Screw Tightening Torques

Terminal Block Connector

Recommended Torque

2-pole

0.5 Nm (4.4 lbf.in)

9-pole

0.2 Nm (1.7 lbf.in)

 
action_zoom_plus_stroke Pluggable screw terminal blocks installed on the CRS-HH-REL-10 relay module
Figure: Pluggable screw terminal blocks installed on the CRS-HH-REL-10 relay module

Show More
action_close

The RP-C-16C-F-230V controller model has PCB mounted connectors for the power input, the input for an external 24 VAC/VDC power supply, the SSR outputs, and the universal inputs/outputs. The PCB mounted connectors mate with pluggable connectors. The PCB mounted connectors are mechanically keyed and color-coded, which allows the matching external connectors to be plugged in on site quickly and easily.

The pluggable connectors mean time savings and cost reductions for the installation, compared to wiring terminal blocks on site. The connectors can quickly and easily be plugged together on site.

The RP-C-16C-F-230V controller uses 2, 3, or 4 pole connectors for the different inputs and outputs.

The connectors are mechanically keyed, which means the following connections cannot be made:

  • A connector for AC mains cannot be plugged into a connector for low-voltage applications.

  • A connector for low-voltage applications cannot be plugged into a connector for AC mains.

The matching connectors are locked together.

The connectors are also color-coded to help the installers and electricians to choose the correct, matching external connector. The connectors are color-coded:

  • Black: For AC mains (230 VAC) power input.

  • White:

    • For 24 VAC/VDC external power supply input.

    • For SSR outputs with 24 VAC/VDC power distribution.

  • Light blue: For universal inputs/outputs (which are designed for low-voltage applications).

  • Turquoise blue: For configurable I/Os (which can be configured either as SSR outputs or universal inputs/outputs).

 
action_zoom_plus_stroke Color-coded connectors
Figure: Color-coded connectors

The matching external connectors are not provided but need to be ordered separately from Schneider Electric. For more information, see Required External Connectors for the RP-C-16C-F-230V Controller Model .

To remove an external connector from an RP controller expansion module or RP-C-16C-F-230V controller
  1. Use a small screwdriver to press and hold down the connector locking tab and then gently pull the external connector until the tab is released from the locking latch (slot).

     
    action_zoom_plus_stroke

  2. Pull the external connector straight away from the mating connector.

     
    action_zoom_plus_stroke
  • RP Controller Expansion Module Pluggable Connectors
  • RP-C-16C-F-230V Pluggable Connectors
  • Plugging an External Connector into an RP Controller Expansion Module or RP-C-16C-F-230V Controller
  • Required External Connectors for the RP Controller Expansion Modules
  • Required External Connectors for the RP-C-16C-F-230V Controller Model
  • RP Controller Expansion Module Device Installation
  • RP-C Models