earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
5
How to

How to


Products: Enterprise Central, Virtual Project Servers
Functionalities: User Management
Product version: 3.1, 3.2, 3.3, 2022, 2023, 2024, 7.0
6/12/2025

Setting an EcoStruxure PCT Server to Password Reset Mode

You set an EcoStruxure PCT Server to password reset mode so that you can create a new password if the old one was forgotten.

Show More
action_close

You can reset the administrator password on your EcoStruxure Building Operation servers. Related information can be found in the sections after the flowchart.

 
action_zoom_plus_stroke Password Reset Workflow
Figure: Password Reset Workflow
Set the server in password reset mode

In Device Administrator, set the Enterprise Server, Enterprise Central and automation server in reset mode.

For more information, see Setting an EcoStruxure BMS Server to Password Reset Mode .

In Project Configuration Tool, set the Project Configuration Tool server in reset mode.

For more information, see Setting an EcoStruxure PCT Server to Password Reset Mode .

Copy the session ID

In WorkStation, copy the session ID that you need to get a temporary password.

For more information, see Copying the Session ID when Resetting the Password .

Send the session ID to Schneider Electric Buildings support team

Contact your local Schneider Electric Buildings support team and send them the session ID.

Create a new password

Log on to the server using the temporary password supplied by Schneider Electric Buildings support team and create the new password.

For more information, see Resetting the Password using WorkStation .

To set an EcoStruxure PCT server to password reset mode
  1. In the Project Configuration Tool, select the server.

  2. Right-click the server and click Set the server in password reset mode .

The PCT server is now in password reset mode for 24 hours.

  • Password Reset Workflow
  • Connecting to an Automation Server Using the USB Device Port
  • Connecting to an Automation Server Using the IP Network
  • Copying the Session ID when Resetting the Password