Our site will be unavailable from October 29-30 due to scheduled maintenance.
Thank you for your patience.
Use the Semantic Settings dialog box to configure the communication between the EcoStruxure BMS server and the Semantic database.
|
Component |
Description |
|
Semantic DB URL |
Enter the address to the semantic database. After you have entered a new database address, you must upload ontologies and restart WorkStation. For more information, see Uploading Ontologies . |
|
Repository |
Type the name to the repository on the semant ic databa se you want to use. |
|
Username |
Enter the username of the EBO user that you want to use to connect with the semantic database. |
|
Password |
Type the password of the EBO user that you want to use to connect to the semantic database.
|
|
Confirm password |
Confirm the password for the EBO user. |
|
Query Timeout |
Enter the timeout the EBO server uses for normal queries against the semantic database. |
|
Update Timeout |
Enter the timeout the EBO server uses for uploading ontologies to the semantic database. |
|
Search Timeout |
Enter the timeout the EBO server uses for search queries against the semantic database. |
|
Export Timeout |
Enter the timeout the EBO server uses for export queries against the semantic database. |
|
Insert Batch Size |
Enter the maximum batch size of files imported to the EBO server from the semantic database. |
|
Lead object |
The lead-shadow mechanism is automatically configured for the semantic database in all EBO servers in the system. You should not change this if you use the same semantic database for the whole EBO system.
|