earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: AS-B, Device Administrator, AS-P
Functionalities: Hardware, License Management
Product version: 2022
10/2/2024

Adding an Entitlement without the HTML file when Automation Server is Connected to License Server (FNO)

You add the entitlement to view the License Products available for activation on automation servers.

Show More
action_close

Device Administrator is used to manage licenses on automation servers.

Licenses on Automation Servers

The following features of an automation server need licenses.

SmartDrivers

To be able to use SmartDrivers on an automation server one license is needed for every SmartDriver that runs on the automation server.

SNMP Notifications

To be able to use SNMP Notification on an automation server, a license is required.

For a stand-alone automation server, the license is local for the automation server and administered by Device Administrator.

In a multi-server system, you can use inherited licenses.

For more information, see Inherited Licenses .

Personal Dashboards

To be able to create personal dashboards on an automation server, you need a license. Personal dashboards are used in WebStation.

For a stand-alone automation server, the license can be local for the automation server and administered by Device Administrator.

In a a multi-server system, you can use inherited licenses.

For more information, see Inherited Licenses .

TimescaleDB

To be able to use TimescaleDB on an automation server, a license is required.

For more information, see Inherited Licenses .

MQTT

To be able to read and write to an MQTT broker from an MQTT client on an automation server, you need a license. For a stand-alone automation server, the license is local for the automation server and administered by Device Administrator.

In a multi-server system, you can use inherited licenses.

For more information, see Inherited Licenses .

Entitlements, Products, and Licenses

Licenses are bought as products and delivered in Entitlements. An Entitlement is a container that can contain several products. The products contain the licenses and they can differ in quantity and contents.

Automation Server Licensing Workflow

Use this workflow to add licenses to automation servers using Device Administrator.

For more information, see Automation Server Licensing on Automation Servers Connected to Internet Workflow .

Certificates

It is recommended to use HTTPS for the communication between Device Administrator and automation servers when you manage licenses.

For more information, see Certificates in Device Administrator .

To add an entitlement without the HTML file when automation server is connected to License Server (FNO)
  1. In Device Administrator, click Entitlements .

  2. Click the Add Entitlement down arrow and click Manually .

  3. Enter the entitlement ID.

  4. Click Next .

  5. Click Add .

  • Automation Server Licensing Overview
  • Order Information Request
  • Licenses Activation Server
  • Add Entitlement Dialog Box
  • Assign Licenses View
  • Assigning Licenses
  • Activating Licenses Online
  • Adding an Entitlement using the HTML file when Automation Server is Connected to License Server (FNO)
  • Automation Server Licensing on Automation Servers Connected to Internet Workflow
  • Automation Server Licensing on Automation Servers not Connected to Internet Workflow