Our site will be unavailable from October 29-30 due to scheduled maintenance.
Thank you for your patience.
Use this workflow to assign and activate licenses on automation servers that do not have any access to Internet.
Related information can be found in the sections after the flowchart.
Install certificates if you use HTTPS for communication.
For more information, see Device Administrator Certificate Workflow .
Make sure that you have the Entitlements containing the licenses. You need the email with the entitlement during the process.
For more information, see Order Information Request .
In Device Administrator, you add entitlements that contains products and licenses.
This is done so that you can view all licenses that are available to be assigned and then activated.
Make sure that you have the HTML entitlement certificate file or the entitlement ID available .
There are two different procedures to add and set up an entitlement:
When the HTML entitlement certificate file is available.
For more information, see Adding an Entitlement using the HTML file when Automation Server is not Connected to License Server (FNO) .
When the HTML entitlement certificate file is not available you must use the entitlement ID.
For more information, see Adding an Entitlement without the HTML file when Automation Server is not Connected to License Server (FNO) .
Use the License Products available in the entitlements to assign License Features to the automation servers.
For more information, see Assigning Licenses .
In Device Administrator, create the request files.
For more information, see Creating the Request Files .
Using Device Administrator, activate request files on License Activation Server (FNO) to receive response files. To be able to complete this procedure, you must be on a computer that is connected to License Activation Server (FNO) via the Internet and have Device Administrator installed.
For more information, see Activating Request Files to Receive Response Files .
Using Device Administrator, send the response files to the automation server to complete the license activation.
For more information, see Sending the Response Files to the Automation Server .
After the licenses has been installed, make a backup of the automation server to make sure that you do not lose the licenses if any problems occur.
For more information, see Backup .