earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Device Administrator, AS-P
Functionalities: Hardware, License Management
Product version: 2022
2/26/2025

Add Entitlement from File

Use the Add Entitlement from file dialog box to add the entitlement.

 
action_zoom_plus_stroke Add Entitlement from file dialog box
Figure: Add Entitlement from file dialog box

Table: Add Entitlement from File Dialog Box

Command

Description

Browse

Browse to the entitlement file.

  • Automation Server Licensing on Automation Servers Connected to Internet Workflow
  • Automation Server Licensing on Automation Servers not Connected to Internet Workflow
  • Add Entitlement from ID
  • Checking Entitlement Dialog Box
  • Contacting License Activation Server Dialog Box