earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Builder View
Functionalities: Engineering
Product version: 2023
11/30/2023

Builder View

arrow1_rotationLive Mode arrow1_rotationCanvas

Builder View is a graphic binding and engineering tool, which allows users of EcoStruxure BMS to graphically view bindings on a canvas between canvas objects properties, and to monitor and follow data flows. Builder View displays objects that are located in the selected current folder structure, and also displays objects outside the current folder structure that are bound to objects within the current folder structure. The bound canvas objects have exposed property names that are displayed as binding ports.

For more information, see Builder View Overview .

Live Mode

In Builder View Live Mode, you display your canvas objects to be able to see the exposed source and target properties for the objects.

Important:

In Live Mode, it is not possible to make changes to the program layout.

For more information, see Live Mode .

Canvas

The canvas in Builder View displays objects that are located inside the selected folder structure in the system tree, or objects outside the selected folder structure, which are bound to objects inside the selected folder structure, and also bindings between the canvas objects. The bound canvas objects have exposed property names that are displayed as binding ports.

For more information, see Canvas .

  • Builder View Overview
  • Live Mode
  • Canvas