earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Builder View
Functionalities: Engineering
Product version: 2023
11/30/2023

Builder View Overview

arrow1_rotationBuilder View arrow1_rotationCanvas Objects

Builder View is a graphic binding and engineering tool, which allows users of EcoStruxure BMS to graphically view bindings on a canvas between canvas objects properties, and to monitor and follow data flows. Builder View displays objects that are located in the selected current folder structure, and also displays objects outside the current folder structure that are bound to objects within the current folder structure. The bound canvas objects have exposed property names that are displayed as binding ports.

Builder View

Builder View is the visual configuring environment integrated into Workstation that allows users of EcoStruxure BMS to view bindings between canvas objects, and to monitor, and follow data flows.

For more information, see Builder View .

Canvas Objects

In Builder View, the visual structure of canvas objects is designed to make the configuration of the objects seamless.

A canvas object can be a:

  • System object

  • Folder object

  • Folder object with system objects in the underlying folder structure

  • External source port

  • External target port

  • Current folder property

For more information, see Canvas Objects .

  • Builder View
  • Canvas Objects