earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Builder View
Functionalities: Engineering
Product version: 2023
11/30/2023

Canvas

arrow1_rotationCanvas Live Mode

The canvas in Builder View displays objects that are located inside the selected folder structure in the system tree, or objects outside the selected folder structure, which are bound to objects inside the selected folder structure, and also bindings between the canvas objects. The bound canvas objects have exposed property names that are displayed as binding ports. For more information, see Canvas Objects .

Canvas Live Mode

On Canvas in Builder View Live Mode, you display your canvas objects to be able to see the exposed source and target properties for the objects.

For more information, see Canvas Live Mode .

  • Builder View
  • Canvas Objects
  • Canvas Live Mode