earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Alarms
Product version: 7.0
12/19/2024

XLSX Report Other Settings Tab

Use the XLSX Report Other Settings tab for various settings.

 
action_zoom_plus_stroke XLSX Report Other Settings Tab
Figure: XLSX Report Other Settings Tab

Table: XLSX Report Other Settings Tab

Component

Description

Enable

Select to enable the XLSX report.

Time range

Select the time range for the XLSX report.

Time zone type

Select Server time zone to display the localized time from the server where the XLSX report is located.

Select Custom time zone to display the custom time zone. If Server time zone is selected, Custom time zone is ignored and not displayed.

Time zone

Select the time zone.

First day of week

Select the day to be set as the first day of week.

Localization

Select a language among the language packs installed on the EcoStruxure BMS server.

Time stamp format

Type the format of date and time that you want to use in the XLSX report.

Decimal count

Select the number of decimals you want to include in the XLSX report.

System of measurement

Select the system of measurements to be used in the XLSX report.

Sort order

Select the sort order used in the XLSX report.

Substitute missing data with

Enter the text that is displayed when a value is missing. By default, a missing value display nothing at all.

  • XLSX Reports Overview
  • XLSX Reports Workflow
  • XLSX Report Template Tab
  • XLSX Template Tab
  • XLSX Report Trigger Settings Tab
  • Context Configuration – Template Tab
  • Context Configuration – Calculation Tab
  • Context Configuration – Misc Tab