earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WebStation
Functionalities: Schedules
Product version: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
5/18/2018

Editing the Status for an Event in a Digital Schedule

You change the status for an event in a digital schedule to control the output state of a digital device at specified times.

Show More
action_close

A digital schedule controls a device that has an on output state and an off output state.

For example, you can create a digital weekly schedule that is bound to a digital output, such as a light switch. To turn on the lights Monday through Friday from 08:00 to 17:00, you can set the value to On when the schedule is active and Off when the schedule is inactive.

 
action_zoom_plus_stroke Digital Schedule
Figure: Digital Schedule

To edit the status for an event in a digital schedule
  1. In WebStation, in the System Tree pane, select the schedule with the event you want to edit.

  2. In the Schedule workspace, navigate to, and then select the schedule event you want to edit.

  3. In the Schedule event properties dialog box, edit the value.

  4. Click OK .

  5. Click Save .

  • Digital Schedules
  • Schedule Editor in WebStation
  • Schedule Workspace Toolbar
  • Weekly Events in WebStation
  • Exception Events in WebStation
  • Editing the Value for an Event in an Analog Schedule
  • Editing the State for an Event in a Multistate Schedule
  • Schedule Workspace
  • Schedule Event Properties Dialog Box – Weekly View
  • Schedule Event Properties Dialog Box – Single Date Exception View
  • Schedule Event Properties Dialog Box – Date Range Exception View
  • Schedule Event Properties Dialog Box – Date Range Exception View
  • Schedule Event Properties Dialog Box – Calendar Reference View