earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WebStation
Functionalities: Schedules
Product version: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
5/18/2018

Editing the Value for an Event in an Analog Schedule

You change the value for an event in an analog schedule to control the output state of an analog device at specified times.

Show More
action_close

An analog schedule controls a device that gauges the output in real numbers. The real numbers include positive or negative numbers, fractions, and decimal values.

For example, you can create an analog schedule to regulate a thermostat setpoint in an office area. To control the temperature from 08:00 to 17:00, you can set the value to 22 °C (72 °F) when the schedule is active and 16 °C (62 °F) when the schedule is inactive.

 
action_zoom_plus_stroke Analog Schedule
Figure: Analog Schedule

To edit the value for an event in an analog schedule
  1. In WebStation, in the System Tree pane, select the schedule with the event you want to edit.

  2. In the Schedule workspace, navigate to, and then select the schedule event you want to edit.

  3. In the Schedule event properties dialog box, in the Value box, enter the new value

  4. Click OK .

  5. Click Save .

  • Analog Schedules
  • Schedule Editor in WebStation
  • Schedule Workspace Toolbar
  • Weekly Events in WebStation
  • Exception Events in WebStation
  • Editing the Status for an Event in a Digital Schedule
  • Editing the State for an Event in a Multistate Schedule
  • Schedule Workspace
  • Schedule Event Properties Dialog Box – Weekly View
  • Schedule Event Properties Dialog Box – Single Date Exception View
  • Schedule Event Properties Dialog Box – Date Range Exception View
  • Schedule Event Properties Dialog Box – Calculated Exception View
  • Schedule Event Properties Dialog Box – Calendar Reference View