earth_america
user_standard Log on
action_search_stroke
earth_america

Hardware

Refine your search
arrow2_down
Refine your search
Ok
Ok
Ok

368 Topic(s)

Concept

The override switches on Central IO modules with manufacturing date earlier than 2021-W26 must be disabled to remove the risk of an improper output. To disable the override switches, update the Central IO module firmware to version 2.017 or later.

Concept

The RTD-DI-16 module is an RTD temperature, RTD resistance, digital, counter, or resistance input, 16-channel I/O module. Each channel has a dedicated two-color (red and green) status LED.

Concept

For I/O modules with outputs, the following components on the front provide control of the output channels:

Concept

Twisted Pair Adapter supports Ethernet over twisted pair cable networks.

Concept

SpaceLogic™ Twisted Pair Adapter - Ethernet (TPA-E) connects to the SpaceLogic BACnet/IP controller and automation server via Ethernet 10/100 Mbit (IEEE 802.3) and utilizes existing twisted pair cabling originally used for legacy serial and free topology protocols. This enables seamless integration of existing twisted pair networks into the IP-based infrastructure of the EcoStruxure Building Management System (BMS), reducing installation costs and simplifying the transition from legacy systems, such as LonWorks FTT-10 networks, to the EcoStruxure BMS network.

Specifications

Specifications

Specifications

Specifications

How to

You wire the terminal blocks installed on the IP-IO module to connect I/O devices and power.