15 Topic(s)
SpaceLogic Sensors are a family of living space sensors designed for BACnet/IP controllers using the EcoStruxure Building Operation user interface. These sensors use an RJ-45 sensor bus that provides communication and power from the BACnet/IP controller.
SpaceLogic Sensor devices are modular and are ordered in two parts: the sensor base and the cover. Four SpaceLogic communicating sensor base models are available as well as a variety of covers.
Use the SpaceLogic Sensor LCD Temperature Sensor model Default screen to advance through the menus, increase and decrease temperature, change modes and degree types, and perform occupany overrides.
Use the SpaceLogic Sensor LCD Temperature Sensor model Degree Type screen to view and configure the degree type setting.
Use the SpaceLogic Sensor LCD Temperature Sensor model Fan Speed screen to view and configure the current fan speed.
Use the SpaceLogic Sensor LCD Temperature Sensor model Heating and Cooling Mode screen to view and configure the current heating or cooling setting.
Use the SpaceLogic Sensor LCD Temperature Sensor model Home or default screen to view the current temperature.
Use the SpaceLogic Sensor LCD Temperature Sensor model Occupancy mode screen to view and configure the room occupancy mode.
The LCD Temperature Sensor model is the relatively inexpensive, mid-range model with a small LCD display and three buttons to increment (plus), decrement (minus) and then select options (middle button) as you scroll through its menus.
SpaceLogic Sensor include blank cover and occupancy sensor-only cover models, as well as several models with pushbutton or display-driven user interfaces that allow you to control temperature, occupancy, overrides, and a variety of other settings in a designated living space.