97 Topic(s)
There are a number of different clients, servers, and features that requires licenses to operate.
A number of software and features need licenses.
(the “EULA”)
License Activation Server, sometimes called FNO server, is a server controlled by Schneider Electric globally to manage the activation of licenses on customers' License Servers.
The License Settings dialog box is used to view the license settings when troubleshooting. Do not change the settings in this dialog. Changes in this dialog results in license violation. The dialog looks different depending on if it is opened from the Other menu in the Show Licenses view toolbar, or if it is opened from the Entitlements View.
Use the Entitlements view to view entitlements.
You activate EcoStruxure Building Operation software licenses, from the License Activation Server, to make EcoStruxure Building Operation software licenses available.
Licenses are needed for EcoStruxure Building Operation products and features that run on Windows.
It is recommended that License Administrator and License Server run on the same computer as Enterprise Server or Enterprise Central that use the licenses.