190 Topic(s)
Use the Policies tab to edit the policies for the domain. For example, the number of failed logon attempts a user can make before the account is temporarily locked.
You set an EcoStruxure PCT Server to password reset mode so that you can create a new password if the old one was forgotten.
Use the Type permissions view to grant user accounts or user account groups extended access to a specific type.
SpaceLogic™ Operator Display is a touch-screen Human Machine Interface (HMI) for SpaceLogic controllers and servers, designed for local monitoring of building controllers in small and medium-sized buildings, as well as in large buildings with comprehensive building management systems. Operator Display is specifically designed for equipment rooms and it simplifies operations, service, and troubleshooting for System Integrators and Service Engineers, as well as for non-technical users (notably Facility Managers and Janitors).
Relative path permissions for a folder structure grant a specific set of permissions to a user account group or to a user account to all the folders accessible in a predefined path and its folder structure. Relative path permissions enable a user accounts group or a user account to reuse a specific path permission.
You create a type permissions template to grant user accounts or user account groups extended access to a specific type.
You can manage user accounts on a domain controller by logging on to the local domain of the EcoStruxure BMS server, using the local administrator and local reports administrator accounts.
Use the Operator Display Settings screen to configure Operator Display and perform administrative tasks.
You force users to change their passwords to strengthen the security in the system.
Use the Appearance tab to configure user settings such as language, time, and display mode.