You commission Zigbee devices from the eCommission SmartX Controller mobile application when Zigbee network and logical devices are configured on your SmartX IP controller.
When the Relay 10 module is configured on the RP-C, you can log into the eCommission SmartX Controller mobile application and configure the following inputs and outputs:
You install SmartX Zigbee Adapter in a dropped ceiling and connect the adapter to an RP-C controller, SmartX AS-P server, or SmartX AS-B server to add Zigbee wireless connectivity to the controller or server.
You install SmartX Zigbee Adapter on a wall using the mounting cradle and wall plate and connect the adapter to an RP-C controller, SmartX AS-P server, or SmartX AS-B server to add Zigbee wireless connectivity to the controller or server.
You install SmartX Zigbee Adapter on the exterior of a metal enclosure and connect the adapter to an RP-C controller, SmartX AS-P server, or SmartX AS-B server to add Zigbee wireless connectivity to the controller or server.
You remove the synchronized BACnet interface of a Child server from its Parent server when you want to independently manage the BACnet interface of the Child server. Should this state later change, you can reassociate the child server BACnet interface with its parent. Child and Parent servers follow the Lead and Shadow relationship. Upon hosting, the Child server automatically propogates with the BACnet interface of the Parent server.