Running the Commission mobile application on a Windows laptop computer, you can connect directly to an Ethernet port on a networked BACnet/IP controller, or use an Ethernet switch to connect to a group of controllers.
Configuration Menus are a group of pre-engineered objects and values that make device commissioning faster and easier. Configuration Menus are exported and downloaded from image files. Download a Configuration Menu to a BACnet/IP controller to commission the controller.
After downloading the configuration menu to the controller, you view and modify the device properties from the configuration menu to complete device commissioning.
The universal inputs/outputs are ideal for any mix of temperature, pressure, flow, status points, and similar point types in a building control system.
You view an I/O checkout report when checkout of all objects in the controller is complete. The report is created when you are performing I/O checkout and select the Save button. The report is saved in the BACnet/IP controller within diagnostic files.