earth_america
user_standard Log on
earth_america

MP-V

Refine your search
arrow2_down
Refine your search
Ok
Ok
Ok

83 Topic(s)

How to

You install the MP-V directly over the VAV damper shaft for damper positioning control and air flow sensing. When you install the MP-V on a damper that rotates clockwise (CW) to open, use WorkStation or the eCommission SmartX Controllers mobile application to ensure that the configured direction of the actuator rotation matches the damper type.

Concept

The wiring recommendations provide guidance regarding wiring of the I/O modules, SmartX servers, and MP Series controllers.

User Interface

The Status LED on the front of the SmartX devices changes color and flashes to indicate the status of the device.

Concept

The I/O wiring recommendations provide guidance on what type of wires should be used for the different I/O modules, SmartX AS-B server onboard I/O, and MP Series controller onboard I/O, how to perform grounding, and how to connect different external devices to the inputs and outputs. Always use the recommended cables and wires.

Concept

The Schneider Electric hardware devices for the EcoStruxure BMS include terminal bases, PS-24V power supplies, SmartX servers such as SmartX AS-P servers and SmartX AS-B servers, MP Series controllers such as MP-Cs and MP-Vs, I/O modules, and ADs.

Concept

It is important to perform the grounding correctly for the following reasons:

Concept

There are many different kinds of external devices from different vendors that can be connected to an EcoStruxure BMS.

Specifications

Concept

The MP-V has a built-in power supply designed to accommodate 24 VAC at 50/60 Hz input power.

How to

You can select the Feedback option to rate your experiences and provide detailed information on the Commission mobile application.