earth_america
user_standard Log on
action_search_stroke
earth_america

RP-V

Refine your search
arrow2_down
Refine your search

148 Topic(s)

Concept

The CRS-HH-REL-10 relay module connects to the RP controllers and enables the control of lights and blinds.

Concept

The RP-V-5C-M model has five I/O points and the controller is equipped with 11 fixed screw terminals and a 3-position removable screw terminal block.

Concept

The RP-V-5A model has five I/O points and the controller is equipped with 11 fixed screw terminals.

Concept

The RP-V-4A model has four I/O points and the controller is equipped with 11 fixed screw terminals.

Concept

The RP-V has fixed screw terminals for the power input, SSR outputs, and universal inputs/outputs. The RP-V-5C-M model also has a removable screw terminal block for connection to the BACnet MS/TP (RS-485) network.

Concept

You must configure the DIP switches as part of the commissioning process for RP controllers that support MS/TP communications.

How to

You install an RP controller expansion Insight-Sensor on an octagon junction box using the supplied mounting ring to properly fasten the Insight-Sensor to the junction box.

How to

You install an RP controller expansion Insight-Sensor on a ceiling using the supplied mounting ring to properly fasten the Insight-Sensor on the ceiling.

How to

You install an RP controller expansion Insight-Sensor into a dropped ceiling using the mounting springs to properly fasten the Insight-Sensor to a ceiling tile.

Concept

The wiring recommendations provide guidance regarding wiring of the Central IO modules, automation servers, RP and MP controllers, IP-IO modules, RP controller expansion modules, and Operator Display.