29 Topic(s)
Use the Enterprise Server viewto start and stop the Enterprise Server service and configure the ports of the Enterprise Server.
Before upgrading the system, it is strongly recommended that you archive the historical data and back up the EcoStruxure BMS servers to preserve the current data and configurations. If you plan to upgrade WebReports, be sure to back up the Reports database in SQL Server.
You uninstall an Enterprise Server to permanently remove the application from your computer.
To uninstall an EcoStruxure Building Operation product you use the Windows Add Remove Program tool. The Windows Add Remove Program tool permanently removes the EcoStruxure Building Operation product from the computer or server.
Use the Enterprise Central viewto start and stop the Enterprise Central service and configure the ports of Enterprise Central.
The Software Administrator installs with the Enterprise Server and Enterprise Central installation package. You use the Software Administrator to start and stop the server service and configure the ports of the Enterprise Server and Enterprise Central.
You start Software Administrator to be able to configure the port settings of the Enterprise Server or Enterprise Central.
You start Enterprise Central manually if it has been stopped.
You start the server manually in case you previously have stopped it.
You stop Enterprise Central to configure the port settings or to repair, upgrade, or reinstall Enterprise Central.