earth_america
user_standard Log on
action_search_stroke
earth_america

UI-8/AO-V-4

Refine your search
arrow2_down
Refine your search
Ok
Ok
Ok

45 Topic(s)

Concept

This section outlines the recommended cables and wires, specifying the appropriate wire sizes and lengths for the Central IO modules.

User Interface

The Status LED on the front of the SmartX devices changes color and flashes to indicate the status of the device.

Concept

The override switches on Central IO modules with manufacturing date earlier than 2021-W26 must be disabled to remove the risk of an improper output. To disable the override switches, update the Central IO module firmware to version 2.017 or later.

User Interface

The I/O modules have the following status indicator LEDs on the front of the module:

Concept

The SmartX AS-P server is the successor to Automation Server, and offers several improvements such as enhanced processor performance, increased memory size, dual Ethernet ports, and high-speed USB interfaces. Like the Automation Server, the SmartX AS-P server is a Schneider Electric manufactured embedded device that generally serves as the lowest tier EcoStruxure BMS server within the EcoStruxure BMS. The SmartX server controls and supervises equipment, typically HVAC equipment. SmartX AS-P servers use I/O modules with connected field devices, such as sensors and actuators, to do that.

Concept

The UI-8/AO-4 module combines 8 universal inputs and 4 analog outputs.

Concept

The UI-8/AO-4 and UI-8/AO-V-4 modules combine 8 universal inputs and 4 analog outputs.

Concept

For I/O modules with outputs, the following components on the front provide control of the output channels:

Concept

By adding a variety of I/O and power supply modules, you can use the SmartX AS-P server or Automation Server to tailor the Intelligent Building Management System to your unique requirements.

Specifications