earth_america
user_standard Log on
action_search_stroke
earth_america

Wireless Adapter - Advanced

Refine your search
arrow2_down
Refine your search
Ok
Ok
Ok

11 Topic(s)

Concept

The EcoStruxure Building Operation software supports the major communication protocols in building automation and security management.

Concept

The Schneider Electric SpaceLogic hardware devices for the EcoStruxure BMS include terminal bases, PS-24V power supplies, Central IO modules, automation servers such as AS-P servers and AS-B servers, BACnet/IP devices such as MP-C controllers, MP-V controllers, IP-IO modules, and RP-C controllers, RP controller expansion modules, remote control, KNX Modbus gateway, Bluetooth adapter, Wireless Adapter - Advanced, SpaceLogic Sensor devices, Advanced Display devices, and Operator Display devices.

Hardware Installation

Concept

Wireless Adapter - Advanced is a USB-based wireless adapter that enables ZigbeeTM wireless connectivity with an RP controller or automation server, extending the controller's or server's point count and bringing flexibility in retrofit applications.

How to

You commission Zigbee devices from the Commission mobile application when Zigbee network and logical devices are configured on your BACnet/IP controller.

Specifications

Concept

This section provides information on regulatory compliance and approvals for Wireless Adapter - Advanced.

How to

You install Wireless Adapter - Advancedr on a wall using the mounting cradle and wall plate and connect the adapter to an RP-C controller, AS-P server, or AS-B server to add Zigbee wireless connectivity to the controller or server.

How to

You install Wireless Adapter - Advanced in a dropped ceiling and connect the adapter to an RP-C controller, AS-P server, or AS-B server to add Zigbee wireless connectivity to the controller or server.

How to

You install Wireless Adapter - Advanced on the exterior of a metal enclosure and connect the adapter to an RP-C controller, AS-P server, or AS-B server to add Zigbee wireless connectivity to the controller or server.