earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AO-8, AO-V-8, DI-16, DO-FA-12, DO-FC-8, RTD-DI-16, UI-16, UI-8/AO-4, UI-8/AO-V-4, UI-8/DO-FC-4
Functionalities: Hardware
Product version: 3.3, 2022, 2023, 2024
9/2/2025

Central IO Modules

By adding a variety of Central IO and power supply modules, you can use the AS-P server to tailor the Intelligent Building Management System to your unique requirements.

Power and communications are delivered to the automation server and its family of Central IO modules in a common bus, thus allowing them to be plugged together without tools. This simple one-step process involves sliding the modules together using their built-in connectors.

The available Central IO modules are designed to accommodate a fixed number of inputs and outputs. For example, several Central IO modules, such as digital inputs, only support a single electrical type. Other modules, such as digital inputs mixed with digital outputs, support a combination of electrical types. The various modules enable you to select the right combination of points necessary for your project.

The Central IO modules are based on the patented two-piece design. Each Central IO module consists of an electronics module and a terminal base.

 
action_zoom_plus_stroke Central IO module, DO-FC-8-H
Figure: Central IO module, DO-FC-8-H

Electronics Modules

The electronics module is the main component of SpaceLogic devices that are based on the patented two-piece design. The electronics module is installed on a terminal base, which constitutes the second component of the device.

For more information, see Electronics Modules .

Terminal Bases

The terminal bases are used for SpaceLogic devices that are based on the patented two-piece design. The terminal base provides the I/O bus to the electronics module installed on the terminal base as well as to the SpaceLogic device installed to the right (next terminal base in the chain).

For more information, see Terminal Bases .

Central IO Module LEDs

The Central IO modules have the following status indicator LEDs on the front of the module:

  • I/O Module Status LED

  • I/O Channel Status LEDs

For more information, see Central IO Module LEDs .

Override Switches and Potentiometers

For Central IO modules with outputs, the following components on the front provide control of the output channels:

  • Override switches

  • Potentiometers

For more information, see Override Switches and Potentiometers .

Important Information on Central IO Modules with Manufacturing Date Earlier Than 2021-W26

The override switches on Central IO modules with manufacturing date earlier than 2021-W26 must be disabled to remove the risk of an improper output. To disable the override switches, update the Central IO module firmware to version 2.017 or later.

For more information, see Important Information on Central IO Modules with Manufacturing Date Earlier Than 2021-W26 .

External Device Connections

There are many different kinds of external devices from different vendors that can be connected to an EcoStruxure BMS.

For more information, see External Device Connections .

Grounding and Power

It is important to perform the grounding correctly for the following reasons:

  • To design a system that is not harmed by detected minor connection errors.

  • To design a system that works well and is resistant to EMI.

  • To minimize the effects of ground currents that can cause unstable measurements.

For more information, see Grounding and Power .

Input Modules

Input modules support a single electrical type, such as digital or universal inputs. The available input modules include the following:

  • DI-16

  • UI-16

  • RTD-DI-16

For more information, see Input Modules .

Output Modules

Output modules support a number of electrical types, such as digital, tristate, and digital/tristate pulsed outputs, or analog outputs. The available output modules include the following:

  • DO-FA-12 and DO-FA-12-H

  • DO-FC-8 and DO-FC-8-H

  • AO-8 and AO-8-H

  • AO-V-8 and AO-V-8-H

For more information, see Output Modules .

Mixed Modules

Mixed modules support a combination of electrical types, such as universal inputs mixed with digital or analog outputs. The available mixed modules include the following:

  • UI-8/DO-FC-4 and UI-8/DO-FC-4-H

  • UI-8/AO-4 and UI-8/AO-4-H

  • UI-8/AO-V-4 and UI-8/AO-V-4-H

For more information, see Mixed Modules .

  • Central IO Modules Overview
  • Hardware Overview
  • Electronics Modules
  • Terminal Bases
  • Central IO Module LEDs
  • Override Switches and Potentiometers
  • Important Information on Central IO Modules with Manufacturing Date Earlier Than 2021-W26
  • External Device Connections
  • Grounding and Power
  • Input Modules
  • Output Modules
  • Mixed Modules