It is important to perform the grounding correctly for the following reasons:
To design a system that is not harmed by detected minor connection errors.
To design a system that works well and is resistant to EMI.
To minimize the effects of ground currents that can cause unstable measurements.
The following sections provide recommendations for designing a good working system.
This section provides grounding and power recommendations for system configurations with Central IO modules and PS-24V units.
有关更多信息,请参阅 Grounding and Power for Systems with Central IO Modules and PS-24V Units .
This section provides grounding and power recommendations for system configurations with AS-B servers.
有关更多信息,请参阅 Grounding and Power for Systems with AS-B Servers .
This section provides grounding and power recommendations for system configurations with MP controllers.
有关更多信息,请参阅 Grounding and Power for Systems with MP Controllers .
This section provides grounding and power recommendations for system configurations with IP-IO modules.
有关更多信息,请参阅 Grounding and Power for Systems with IP-IO Modules .
This section provides grounding and power recommendations for system configurations with the RP-C controller models that support 24 VAC/VDC input power and have a half-wave rectified and non-isolated built-in power supply.
This section provides grounding and power recommendations for system configurations with the RP-C controller models that support 24 VAC/VDC input power and have a full-wave rectified and isolated built-in power supply.
This section provides grounding and power recommendations for system configurations with the RP-C controller models that support 230 VAC input power.
有关更多信息,请参阅 Grounding and Power for Systems with RP-C 230 V Controller Models .
This section provides grounding and power recommendations for system configurations with the RP-C-16C-F-230V controller model and an external 24 VAC/VDC power supply connected to the EXT Input of the controller.
有关更多信息,请参阅 Grounding and Power for Systems with RP-C-16C-F-230V and External 24 VAC/VDC Power Supply .
This section provides grounding and power recommendations for system configurations with the RP-C controller models that support 230 VAC input power and RP controller expansion modules.
有关更多信息,请参阅 Grounding and Power for Systems with RP-C 230 V Controller Models and RP Controller Expansion Modules .
This section provides grounding and power recommendations for system configurations with the RP-V controllers, which support 24 VAC input power.
有关更多信息,请参阅 Grounding and Power for Systems with RP-V Controllers .
This section provides grounding and power recommendations for system configurations with the RP-IO I/O modules, which support 24 VAC/VDC input power and have a full-wave rectified and isolated built-in power supply.
有关更多信息,请参阅 Grounding and Power for Systems with RP-IO Modules .
This section provides grounding and power recommendations for system configurations with Operator Display, which supports 24 VDC input power.
有关更多信息,请参阅 Grounding and Power for Systems with Operator Display .