earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Automation Server, AS-B, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Basic Functionality
Product version: 1.8, 1.9
10/12/2017

Connect Agent

Connect Agent is the service that runs along with the Enterprise Server to collect and transfer system information and crash information of SmartStruxure servers (Enterprise Server and SmartStruxure server devices attached to it). The system information of the Enterprise Server and all the attached SmartStruxure server devices is backed up at regular intervals and stored in the Enterprise Server. The Connect Agent service then removes the PII (Personally Identifiable Information) from the latest backup and the processed information is sent to the Connect storage server.

To transfer the crash information and system information, the Connect Agent service Log on needs to meet the following conditions:

  • sufficient user rights to access system folders and internet

  • Internet proxy settings, if required

  • Port number 22 available to access the following URLs:

    • servercd.smartstruxure.schneider-electric.com

    • serversi.smartstruxure.schneider-electric.com

Connect Agent can collect and transfer system information and crash information only when the site administrator or the end-user provides consent to allow Schneider Electric to receive system diagnostic and performance data of the system. For more information, see Providing Your Consent on Sharing System Information .

To enable the Connect Agent function, set Enable system information transfer and Enable crash information transfer to True. For more information, see Configuring Connect Agent Settings .

  • Configuring Connect Agent Settings
  • Providing Your Consent on Sharing System Information
  • Backup Rule Properties – Basic Tab
  • Transferring System and Crash Information
  • System and crash information not available on Connect storage server