Our site will be unavailable from October 29-30 due to scheduled maintenance.
Thank you for your patience.
The UL 864 listed MNA-FLO-1 enclosure is a 2.75-inch deep (69.85 mm) box designed for use with VAV controllers.
The following illustration shows the front view of the enclosure.
As shown, the front view includes a product and smoke control label and an enclosure cover.
The following illustration shows the inside view of the enclosure.
As shown, the inside of the enclosure includes a b3/i2865-V-S controller, an enclosure base, a damper shaft, a product label, and a mounting tab.
The MNA-FLO-1 provides knockouts in the positions shown for .50 inches (12.70 mm) or .75 inches (19.05 mm) conduit connections.