Our site will be unavailable from October 29-30 due to scheduled maintenance.
Thank you for your patience.
The SEBOX121806 is a 5.9-inch deep (150 mm) compact, multi-purpose box. Its features include a reversible door with invisible hinges that open 120 degrees, a standard 3mm double bar lock with screw driver lock feature and a foamed-in polyurethane gasket door that prevents water and dust migration. An optional key lock is also available. You can order the enclosures with an optional perforated back platel using the P suffix on the model. The SEBOX121806 is designed for use with EcoStruxure Building Operation components, such as Automation Servers, Power Supplies, MP-X IP controllers and Input/Output modules.
The SEBOX121806 is a wall-mounted enclosure with the following dimensions:
Height: 11.8 inch (300 mm)
Width: 17.7 inch (450 mm)
Depth: 5.9 inch (150 mm)
Cubic inch volume: 1232 (20250 cu. cm)
For more information, see Mounting a UL 864 Smoke Control Enclosure .