Our site will be unavailable from October 29-30 due to scheduled maintenance.
Thank you for your patience.
The SEBOX393210 enclosure is a 9.8 in (250 mm) deep box. Its features include a reversible door with invisible hinges that open 120 degrees, a standard 3mm double bar lock with screw driver lock feature and a foamed-in polyurethane gasket door that prevents water and dust migration. An optional key lock is also available. You can order the enclosures with an optioal perforated back plateanel using the P suffix on the model. The SEBOX393210 is designed for use with EcoStruxure Building Operation components, such as Automation Servers, Power Supplies, MP-X IP controllers and Input/Output modules.
The SEBOX393210 is a wall-mounted enclosure with the following dimensions:
Height: 39.4 inch (1000 mm)
Width: 31.5 inch (800 mm)
Depth: 9.8 inch (250 mm)
Cubic inch volume: 12162 (200000 cu. cm)
For more information, see Mounting a UL 864 Smoke Control Enclosure .