Produits : WebStation
Fonctionnalités : Tendances
Version produit : 2024, 7.0
03/12/2024

Adding a Trend Chart Series to a Trend Chart in WebStation

You add a trend log series to a trend chart to compare trend data from different logs or variables.

Afficher plus
action_close

You can display the trend logs as trend log series in a trend chart in a number of ways. For example, you can change the color and weight of the trend log line, or display markers at the time where the trend log value was sampled.

These settings can be saved so that the trend chart is displayed in the same way anytime you open it.

To add a trend chart series to a trend chart in WebStation 
  1. In WebStation, in the System Tree pane, select the trend chart you want to add a trend log series to.

  2. On the Trend Chart toolbar, click the Add button

     
    action_zoom_plus_stroke
    .

  3. In the Select object dialog box, enter the series you want to add.

  4. Click OK .

  5. Click Save .

  • Trend Chart Series in WebStation
  • Trend Chart Toolbar in WebStation
  • Changing the Color of a Trend Chart Series
  • Changing the Presentation Type of a Trend Chart Series
  • Showing Markers in a Trend Log Series
  • Show Tooltips for All Series in a Trend Chart
  • Removing a Trend Chart Series
  • Saving Current Trend Chart Settings