Trend Chart Series in WebStation
You can display the trend logs as trend log series in a trend chart in a number of ways. For example, you can change the color and weight of the trend log line, or display markers at the time where the trend log value was sampled.
These settings can be saved so that the trend chart is displayed in the same way anytime you open it.
How Trend Charts Work
How Trend Logs Work
Trend Chart View
Trend Chart Toolbar
Trend Chart Settings Dialog Box – Left Axis Tab
Menu Série de la courbe de tendance
Displaying Specific Time Spans of a Trend Chart
Showing Markers in a Trend Log Series
Changing the Line Weight of a Trend Chart Series
Changing the Color of a Trend Chart Series
Changing the Presentation Type of a Trend Chart Series
Show Tooltips for All Series in a Trend Chart
Ajout d'une série de journaux de tendance à une courbe de tendance
Removing a Trend Chart Series
Masquage d'une série dans une courbe de tendance
Saving Current Trend Chart Settings