earth_america
user_standard Accedi
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concetto

Concetto


Prodotti: AS-P Smoke Control, Automation Server Smoke Control
Funzionalità: Smoke Control
Versione del prodotto: 1.8
26/09/2016

Electronics Module Installation

To ensure that the correct electronics module is used with the correct terminal base, you must always check that the warning label on the terminal base backplane indicates which module type should be connected. Write the intended module type, if it is not already printed, on the label.

 
action_zoom_plus_stroke Terminal Base Label (Module Type)
Figura: Terminal Base Label (Module Type)
Allarme Allarme

Unintended equipment operation

Install only the module type that is indicated on the label of the terminal base. If the label does not indicate the intended module type, consult the control panel documentation to determine the intended module type. A mismatch can cause electric shock and damage the electronics module.

Failure to follow these instructions can result in death, serious injury, or equipment damage.

Install an electronics module on a terminal base as follows:

1. Pull out the two handles on the left and right sides of the module

2. Plug the module into the terminal base, ensuring that the PCB header pins align correctly with the backplane socket, and press firmly

3. Push the handles in firmly to lock the module in place

4. Open the clear plastic label carriers

5. Write and insert the labels

6. Close the label carriers

If the PS-24V module is inserted with 24 VAC power applied, the Smoke Control, or I/O module you are installing powers up when plugged in. You should see the status LED activate. Per maggior informazioni, consulta PS-24V Power Supply Module .

  • SmartStruxure Module Installation
  • Terminal Base Installation
  • Power Rating
  • Terminal Base Wiring
  • PS-24V Power Supply Module
  • Automation Server Installation
  • AS-P Installation
  • MS/TP Cable Routing
  • Module Status LEDs
  • I/O Module Installation