earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-B, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Alarms
Product version: 3.2, 3.3, 2022
10/15/2020

Notification Report Example 2

In the system example, we have created Building A and Building B with a number of identical rooms. We have also created a folder for the repeption area in Building A. In the Reception folder, we have created an analog value and a trend log that logs the temperature in the reception area. The value is connected to an alarm. A notification report that contains the log data is to be displayed in a web browser when a user manually triggers the notification.

We have created a variable triggered notification.

 
action_zoom_plus_stroke Variable triggered notification
Figure: Variable triggered notification

We have created a notification report template. The notification report template functions as a template for how notification report content is displayed when the notification is triggered. For more information, see Notification Reports .

The template is configured to be displayed as a simple web page that lists the temperature data in an HTML table.

 
action_zoom_plus_stroke The notification report text in HTML including the trend log data
Figure: The notification report text in HTML including the trend log data

The trend report data is configured to display each log record as a new table row with two cells: Timestamp and Value.

 
action_zoom_plus_stroke The trend log part of the notification report text in HTML
Figure: The trend log part of the notification report text in HTML

We have created a variable triggered notification.

 
action_zoom_plus_stroke Variable triggered notification
Figure: Variable triggered notification

The notification is configured to distribute the notification report as a write to file notification with the HTML file extension. The notification report is generated when a user manually triggers the variable triggered notification that uses the notification report template.

 
action_zoom_plus_stroke The file name in the notification specifies the file type that is to be generated
Figure: The file name in the notification specifies the file type that is to be generated

The file is accessed from the 'Notification Files' folder of the 'System' folder and is opened in a web browser.

 
action_zoom_plus_stroke The notification report opened in a web browser
Figure: The notification report opened in a web browser
  • Notification Reports
  • Notifications
  • Manually Triggering a Notification
  • Notification Report Workflow
  • Notification Report Example 1
  • Creating a Notification Report Template
  • Creating a Variable Triggered Notification