earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos AS-L, AS-B, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Alarmas
Versión del producto: 1.9
06/11/2017

Create Alarm Decoration Rule Wizard - User Action Page

Use the User Action page or tab configure the user action required when the alarm decoration rule conditions are met.

 
action_zoom_plus_stroke User Action page
Figura: User Action page

Tabla: User Action Page or Tab

Property

Description

Override

Select the boxes for the user action properties you want to override when the alarm decoration rule conditions are met.

Cause note group

Enter the cause note group that is used by the alarm when the alarm decoration rule conditions are met.

Para obtener más información, consulte User Actions .

Action note group

Enter the action note group that is used by the alarm when the alarm decoration rule conditions are met.

Para obtener más información, consulte User Actions .

Checklist

Enter the checklist that belongs to the alarm when the alarm decoration rule conditions are met.

Para obtener más información, consulte User Actions .

Required User Actions

Select what actions the user has to perform when any of the listed events occur and when the alarm decoration rule conditions are met.

Para obtener más información, consulte User Actions .

  • Alarm Decoration
  • User Actions
  • Create Object Wizard – Naming the Object Page
  • Create Alarm Decoration Rule Wizard - Filter Page
  • Create Alarm Decoration Rule Wizard - Presentation Page
  • Create Alarm Wizard – Attachment Page