Use the Filter page or tab to configure the conditions that have to be met before the alarm decoration rule overrides the original properties configured for the alarm.
Property |
Description |
![]() |
Add condition Click to add the conditions that have to be met before the alarm decoration rule becomes active and overrides the original configuration of the alarm. Para obtener más información, consulte Cuadro de diálogo Añadir/eliminar Condiciones . |
![]() |
Remove condition Click to remove the selected condition. |
![]() |
Add row Click to add another condition that has to be met before the alarm decoration rule becomes active. |
![]() |
Remove row Click to remove the selected alarm decoration rule condition. |
Clear all |
Click to clear the selected conditions. |