earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Användargränssnitt

Användargränssnitt


Produkter: AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funktionaliteter: Larm
Produktversion: 3.2, 3.3, 2022
2020-10-15

Create Alarm Decoration Rule Wizard - User Action Page

Use the User Action page or tab configure the user action required when the alarm decoration rule conditions are met.

 
action_zoom_plus_stroke User Action page
Figur: User Action page

Tabell: User Action Page or Tab

Property

Description

Override

Select the boxes for the user action properties you want to override when the alarm decoration rule conditions are met.

Cause note group

Enter the cause note group that is used by the alarm when the alarm decoration rule conditions are met.

Mer information finns i User Actions .

Action note group

Enter the action note group that is used by the alarm when the alarm decoration rule conditions are met.

Mer information finns i User Actions .

Checklist

Enter the checklist that belongs to the alarm when the alarm decoration rule conditions are met.

Mer information finns i User Actions .

Required User Actions

Select what actions the user has to perform when any of the listed events occur and when the alarm decoration rule conditions are met.

Mer information finns i User Actions .

  • Alarm Decoration
  • User Actions
  • Create Object Dialog – Naming the Object Page
  • Create Alarm Decoration Rule Wizard - Filter Page
  • Create Alarm Decoration Rule Wizard - Presentation Page
  • Create Alarm Wizard – Attachment Page