earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos WorkStation, Project Configuration Tool
Funcionalidades: Funcionalidad básica, Ingeniería
Versión del producto: 1.9
14/12/2016

Timed Force Digital Object Properties – Basic Tab

Use the Basic tab to configure and view the basic properties of the Timed Force Digital object.

 
action_zoom_plus_stroke Timed Force Digital object properties – basic tab
Figura: Timed Force Digital object properties – basic tab

Tabla: Basic Tab

Component

Description

Value 

Displays the value of the object's output.

Force type select

Select the type of force time.

Force duration

Select the duration of the force in minutes.

Force until

Select the date and time at which the force must end.

Input

Displays the constant or reference value of the input. 

  • Timed Force Digital Object
  • General Information Properties – Basic Tab
  • References Tab
  • Create Object Wizard – Naming the Object Page
  • Timed Force Digital Object Properties – Parameters Tab