earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
功能: BACnet
产品版本: 2024, 7.0
2024/12/3

Configuring State Values in a Timed Force Multistate Object

In a Timed Force Multistate object, you configure one or more state values to define a text string associated with each of those values.

显示更多
action_close

The state configuration of a Timed Force Multistate object allows specific multistate values to be associated with text strings. The result is that for a given state, the value displayed to the user is the text string associated with the particular numeric multistate value.

A Timed Force Multistate object allows up to 256 states to be created. Each of these states has a default text string value of "State [state value]", which can be edited to display an appropriate description of the state, such as "Unoccupied" or "Standby". The state text string can be constructed using any of the characters allowed in the EcoStruxure Building Operation software.

有关更多信息,请参阅 Configuring State Values in a Timed Force Multistate Object .

To configure state values in a Timed Force Multistate object
  1. In WorkStation, in the System Tree pane, locate and then select the Timed Force Multistate object.

  2. Click the State Configuration tab.

  3. Enter the number of states that you want to create.

     
    action_zoom_plus_stroke
  4. On the State Configuration tab, click the Save button

     
    action_zoom_plus_stroke
    .

  5. In the State Definitions list, select a state and then click the Edit button

     
    action_zoom_plus_stroke
    .

  6. Click the Basic tab.

     
    action_zoom_plus_stroke
  7. In the Label box, type a description you want to associate with the state number and then click OK .

  8. On the State Configuration tab, click the Save button

     
    action_zoom_plus_stroke
    .

  9. Repeat steps 5 through 8 for each state that you created.

The states of the Timed Force Multistate object are each configured with text strings. When one of those states is selected and then forced on the object's Basic tab, the text string associated with that state is displayed.

  • Timed Force Multistate Object State Configuration
  • Timed Force Multistate Object Properties – State Configuration Tab
  • Timed Force Multistate Object Properties – Basic Tab
  • Timed Force Multistate Object Properties – Parameters Tab
  • General Information Properties – Basic Tab
  • References Tab