earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concepto

Concepto


Productos MP-C, MP-V
Funcionalidades: Hardware
Versión del producto: 2.0, 2.1, 3.0, 3.1, 3.2
04/02/2019

MP Series Controller Communication Ports

The MP Series controller contains a combination of Ethernet, USB, and SmartX Sensor communication ports.

This combination includes the following ports:

  • Two 10/100 Ethernet ports

  • One USB host port

  • One USB device port

  • One sensor bus port

When both Ethernet ports are enabled, they function as an onboard Ethernet switch. Disabling the second Ethernet port disables the switching function. The switching function enables flexible network topologies. Para obtener más información, consulte SmartX IP Controller Network Topologies . The second port also provides a connection point for a laptop running the eCommission SmartX Controllers mobile application.

The two USB ports are reserved for future use.

The sensor bus port is designed for connection of SmartX Sensors. Para obtener más información, consulte SmartX IP Controller Sensor Bus .

  • Hardware Overview
  • MP-Cs
  • MP-Vs
  • SmartX IP Controller Sensor Bus
  • SmartX IP Controller Network Topologies