Funkcje: Podstawowa funkcjonalność
Wersja produktu: 3.2, 3.3, 2022
2020-10-15

Mass Changing Units

You mass change units of the EcoStruxure Building Operations objects to save time when configuring units.

Pokaż więcej
action_close

Use mass edit when you want to change several property values or rename several objects at a time.

You can change several property values at a time, for example, when you want to change all setpoints from 22 to 20. Więcej informacji zawiera Mass Editing Objects .

 
action_zoom_plus_stroke Multi editing
Rysunek: Multi editing

The objects do not need to be of the same type to be mass edited. However, the properties you want to edit have to be of the same type.

You can mass rename all objects that are possible to move. For example, you can rename alarms but not properties.

You can rename the objects one by one. You can also copy row-separated text from a file, such as an MS Excel file, and paste it to rename several rows in one single operation. When you paste, the copied text is pasted from the row you have clicked and down in the list. If the copied text is longer than the number of rows, pasting stops at the last row.

Więcej informacji zawiera Mass Renaming Objects  .

Więcej informacji zawiera Mass Renaming Objects Using Copy and Paste  .

When you hover over the names in the Name column, the full path of the object is displayed.

You can mass change the units of objects in a search result. Więcej informacji zawiera Mass Changing Units .

To mass change units
  1. In WorkStation, select the container for the objects whose units you want to change.

  2. In the Search View , type a common name or part of name of the objects you want to search for.

  3. Select the Search for properties box.

  4. In the Property name box, enter the name of the property whose unit you want to change.

  5. In the search result list, select the properties whose units you want to change.

  6. Right-click and then click Select unit .

  7. In the Select Unit dialog box, select the unit from the list and click Select .

The unit properties of the objects are immediately changed in the database.

  • Mass Edit
  • EcoStruxure Building Operation Objects
  • List View
  • List View Context Menu
  • Search View
  • Search Results List Context Menu
  • Select Unit Dialog Box